SLVAFJ3 september   2023 LM5177 , LM51772

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Importance of DC-DC Power Supply Layout
  5. 2Steps for a Good Layout
    1. 2.1 Identifying Critical Circuit Paths
    2. 2.2 Optimizing Hot Loops in the Power Stage
    3. 2.3 Separating Differential Sense Lines From Power Planes
      1. 2.3.1 Using Net Ties to Separate Routing
    4. 2.4 Routing Gate-Drive and Return Paths
    5. 2.5 Controller Layout
    6. 2.6 Separate AGND and PGND
    7. 2.7 Thermal Vias
  6. 3Tips for Layout Optimization
  7. 4Layout Example
  8. 5Summary
  9. 6References

Tips for Layout Optimization

  • Do the placement of the power circuit first.
    • Change part locations, and importantly the orientations, to make the high current flow along a short and straightforward path. Prevent unnecessary zigzag patterns.
    • Try to avoid using via holes on the high current path unless they are necessary. When using vias, you need to use an adequate number of via holes.
    • There is a tradeoff to make among the number of, and spacing between, the via holes. Too many via holes crowded in a small area can hinder current flow due to the loss of copper area.
  • Find a location for the controller IC, not too far from the MOSFETs that it will drive. The location needs to allow a decent AGND polygon to accommodate all control signals. The AGND and PGND connection point needs to be the thermal pad. Place the critical control components next to the controller IC, and visualize the signal routes. Move the components and change their orientations to simplify the routing
  • Route high current traces as well as the critical control signal paths before routing other traces.
  • Optimal layout of the switch mode power supply is always the result of iterations. There is no short cut that can lead to an optimal layout in one shot.