SLVUCP9A November 2023 ā March 2024 TPS25751
The Application Customization Tool is used to directly load a configuration onto the TPS25751EVM. Connect J4 Type-C connector with a cable (both USB-A to USB-C or USB-C to USB-CĀ® cables work) to a laptop or computer with the Application Customization Tool open. Make sure the TPS25751EVM is properly powered either through J2 Type-C connector to a 15V-20V Type-C adapter or with a bench power supply. See the figure below for reference.
Open the Application Customization Tool and complete the questionnaire, refer to Section 3.3.3 for details on each question. Once the questionnaire is complete and the TPS25751EVM is connected properly, click on Options ā Serial Port Configuration to make sure the correct COM port is selected. See the figure below for reference.
If the TPS25751EVM is unable to connect to the Application Customization Tool, then go through the following debug recommendations:
Once the questionnaires are completed and the TPS25751EVM is connected to the Application Customization Tool, click on Flash To Device ā Flash to device from current configuration.