SNAS693D July 2017 – February 2021 HDC2010
PRODUCTION DATA
The HDC2010’s relative humidity-sensing element is located on the bottom side of the package.
TI recommends that the user eliminate the copper layers below the device (GND, VDD) and create slots in the PCB around the device to enhance the thermal isolation of the HDC2010. To ensure the temperature sensor performance, TI highly recommends that the user follow the Land Pattern, Solder Mask, and Solder Paste examples depicted in the Figure 10-1.