SPRACV2 November 2020 AWR1843 , AWR2243
The API AWR PHASE SHIFTER CAL DATA RESTORE SB can be used to restore the TX phase shifter calibration data into the device in the field operation.
For restoring the estimated phase shift values of the raw analog for the present temperature, send the following to the above API:
The user should account for this API’s phase indexing format, which may differ across TXs (refer to the Appendix Section 7.5).