SPRAD50A August 2022 – March 2023 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1
The QSPI Flash memory can be utilized two different ways in the user system:
When picking a Flash memory IC, the device must comply with all boot requirements of the system-on-chip (SoC). If the memory is used as boot media, some guidelines must be followed to work efficiently as a storage device during application.
Figure 1-1 depicts the Flash memory organization once the secondary bootloader (SBL) image and valid application image are present.