SPRAD70 March 2023 AM2631 , AM2631 , AM2631-Q1 , AM2631-Q1 , AM2632 , AM2632 , AM2632-Q1 , AM2632-Q1 , AM2634 , AM2634 , AM2634-Q1 , AM2634-Q1
#define INA226 (0X01) //1 - INAA26 is used, 0 - INA228 is used
Input the voltage rail that needs to be monitored as shown below:
#define RAIL_1V2 (0x01) //1 - 1.2V rail to be monitored, 0 - 3.3V rail to be monitored
#define INA226_REG_CALIBRATION_MSB_VALUE (0x14) /* Input from user */
#define INA226_REG_CALIBRATION_MSB_VALUE (0x00) /* Input from user */