SPRAD85 March 2023 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1
The AM62A7/AM62A3 family of processors includes wide variety of capabilities, not all of which will be used in every design. Consequently, the requirements for different designs using the same device can vary widely depending on the target application. Designers must understand the requirements before determining the details of the design. In addition, the design may require additional circuitry to operate correctly in the target environment. For the selected device and determine the following, see latest collaterals on TI.com like the device-specific Data Sheet, Errata, TRM and EVM User's guides: