SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The A72SS does not have an integrated watchdog timer. Instead, this feature is provided externally by the Real Time Interrupt (RTI) module, which implements a windowed watchdog timer capable of issuing warm reset to the SoC, when necessary.
There are two RTI modules in the MAIN domain that are assigned to the A72 cores:
For more details on the RTI windowed watchdog feature, see Real Time Interrupt Module (RTI).