SWRU602 September 2023 CC3300 , CC3301
Before running any of the commands, the device and the driver needs to be configured in Production Line Test (PLT) mode. Use the following commands to configure the device to PLT mode:
calibrator wlan0 plt power_mode on
To exit PLT mode use the below command:
calibrator wlan0 plt power_mode off