TIDT363 December 2023
Conducted EMI tests were done in a shielded test chamber.
Radiated EMI tests were done in a CISPR25 conforming shielded test chamber.
For both types of tests, a freshly charged 12-V lead acid battery was used as a power source and a 220-mΩ resistor (Arcol HS100 R22 J) was used as a load, resulting in a load current of 23 A, which is above the targeted 22-A nominal output current. All EMI tests were done with dual random spread spectrum (DRSS) enabled.
The following measurements were done: