TIDUBY9 December 2021
Magnetic tampering testing was performed by using a strong 0.5 in diameter × 1.5 in thick N52 cylinder magnet. The magnet was applied underneath the trigger module because that location is most susceptible to external magnetic fields due to that location having the shortest possible distance from the Hall sensors to any external magnets that are placed on the trigger module.
The two magnet orientations shown in Figure 2-11 and Figure 2-12 were tested. For the different magnet orientations of the external magnet, it was verified that the system did not turn ON by making sure that the LPWR LED did not turn ON. For more information on which Hall sensors were triggered by the different magnet orientations, the individual LEDs on switches U1, U2, U3, and U4 were also observed.