Import the application project by selecting Menu → Project → Import CCS Projects, and then select the following path: <USS Flow Meter Library folder>\examples\USSLib_GUI_Demo\CCS\ (see Figure 4-13).
Figure 4-13 Import Project to CCS
Build the project (Ctrl+B).
Download the code to the device (F11).
Close the debugger. It is also possible to execute or debug the application, but this design guide only shows the standalone execution.