TIDUEZ6 December 2021 TPS62912 , TPS62913
The TIDA-010230 clocking board includes the FTDI device, which needs to be programmed once to support the SW GUI. An FTDI utility, FT Prog, is installed from the web. Figure 2-3 shows the product description is set to the TIDA010230.
The TIDA-010230 GUI interfaces with the TIDA-010230 clocking hardware to configure all clocking devices on the board. Install this software from the Software section of the TIDA-010230 reference design folder.