TIDUF13 November 2022 ADS117L11 , ADS127L11
The board relies on an onboard LDO to supply the required 5 V to the analog circuits. The input source is connected to J1, and try valid input range is 5.2 V to 6 V (5.1 V can also be tried)
D2 turns on if the supply is active.
The estimated current from the analog supply is below 100 mA.