SimpleLink Wi-Fi CC3220 and CC3120 Product Overview
01:15:54
|
27 APR. 2017
| This is an overview of SimpleLink for the second generation, which has CC3220 and CC3120 devices. These devices are raising the bar for low power, security, and time to market for any interconnected devices. The number of connected devices in the market is growing exponentially, which means there are more barriers to development than ever before. This video will provide information on how the CC3220 and CC3120 overcome these development barriers. |