SNAS192G April   2003  – May 2016 ADCS7476 , ADCS7477 , ADCS7478
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
    5. 6.5 Electrical Characteristics - ADCS7476
    6. 6.6 Electrical Characteristics - ADCS7477
    7. 6.7 Electrical Characteristics - ADCS7478
    8. 6.8 Timing Requirements
    9. 6.9 Typical Characteristics
  7. 7 Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
    4. 7.4 Device Functional Modes
      1. 7.4.1 Transfer Function
      2. 7.4.2 Power-Up Timing
      3. 7.4.3 Modes of Operation
        1. 7.4.3.1 Normal Mode
        2. 7.4.3.2 Start-Up Mode
        3. 7.4.3.3 Shutdown Mode
  8. 8 Application and Implementation
    1. 8.1 Application Information
      1. 8.1.1 Analog Inputs
      2. 8.1.2 Digital Inputs and Outputs
    2. 8.2 Typical Application
      1. 8.2.1 Design Requirements
      2. 8.2.2 Detailed Design Procedure
      3. 8.2.3 Application Curves
  9. 9 Power Supply Recommendations
    1. 9.1 Power Supply Noise
    2. 9.2 Digital Output Effect Upon Noise
    3. 9.3 Power Management
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11Device and Documentation Support
    1. 11.1 Device Support
      1. 11.1.1 Device Nomenclature
    2. 11.2 Community Resources
    3. 11.3 Trademarks
    4. 11.4 Electrostatic Discharge Caution
    5. 11.5 Glossary
  12. 12Mechanical, Packaging, and Orderable Information

Package Options

Mechanical Data (Package|Pins)
Thermal pad, mechanical data (Package|Pins)
Orderable Information

11 Device and Documentation Support

11.1 Device Support

11.1.1 Device Nomenclature

    APERTURE DELAY

    is the variation in aperture delay from sample to sample. Aperture jitter manifests itself as noise in the output.

    APERTURE JITTER (APERTURE UNCERTAINTY)

    is the variation in aperture delay from sample to sample. Aperture jitter manifests itself as noise in the output.

    DIFFERENTIAL NON-LINEARITY (DNL)

    is the measure of the maximum deviation from the ideal step size of 1 LSB.

    DUTY CYCLE

    is the ratio of the time that a repetitive digital waveform is high to the total time of one period. The specification here refers to the SCLK.

    EFFECTIVE NUMBER OF BITS (ENOB, or EFFECTIVE BITS)

    is another method of specifying Signal-to-Noise and Distortion or SINAD. ENOB is defined as (SINAD - 1.76) / 6.02 and says that the converter is equivalent to a perfect ADC of this (ENOB) number of bits.

    FULL POWER BANDWIDTH

    is a measure of the frequency at which the reconstructed output fundamental drops 3 dB below its low frequency value for a full scale input.

    GAIN ERROR

    is the deviation of the last code transition (111...110) to (111...111) from the ideal (VREF – 1.5 LSB for ADCS7476 and ADCS7477, VREF – 1 LSB for ADCS7478), after adjusting for offset error.

    INTEGRAL NON-LINEARITY (INL)

    is a measure of the deviation of each individual code from a line drawn from negative full scale (½ LSB below the first code transition) through positive full scale (½ LSB above the last code transition). The deviation of any given code from this straight line is measured from the center of that code value.

    INTERMODULATION DISTORTION (IMD)

    is the creation of additional spectral components as a result of two sinusoidal frequencies being applied to the ADC input at the same time. It is defined as the ratio of the power in the either the two second order or all four third order intermodulation products to the sum of the power in both of the original frequencies. IMD is usually expressed in dBFS.

    MISSING CODES

    are those output codes that never appear at the ADC outputs. ADCS747x is ensured not to have any missing codes.

    OFFSET ERROR

    is the deviation of the first code transition (000...000) to (000...001) from the ideal (that is, GND + 0.5 LSB for the ADCS7476 and ADCS7477, and GND + 1 LSB for the ADCS7478).

    SIGNAL TO NOISE RATIO (SNR)

    is the ratio, expressed in dB, of the rms value of the input signal to the rms value of the sum of all other spectral components below one-half the sampling frequency, not including harmonics or DC.

    SIGNAL TO NOISE PLUS DISTORTION (S/N+D or SINAD)

    Is the ratio, expressed in dB, of the rms value of the input signal to the rms value of all of the other spectral components below half the clock frequency, including harmonics but excluding DC.

    SPURIOUS FREE DYNAMIC RANGE (SFDR)

    is the difference, expressed in dB, between the rms values of the input signal and the peak spurious signal, where a spurious signal is any signal present in the output spectrum that is not present at the input.

    TOTAL HARMONIC DISTORTION (THD)

    is the ratio, expressed in dBc, of the rms total of the first five harmonic levels at the output to the level of the fundamental at the output. THD is calculated as:

    Equation 1. ADCS7476 ADCS7477 ADCS7478 20057799.png

    where

    • f1 is the RMS power of the fundamental (output) frequency
    • f2 through f6 are the RMS power in the first 5 harmonic frequencies
    TOTAL UNADJUSTED ERROR

    is the worst deviation found from the ideal transfer function. As such, it is a comprehensive specification which includes full scale error, linearity error, and offset error.

11.2 Community Resources

The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.

    TI E2E™ Online Community TI's Engineer-to-Engineer (E2E) Community. Created to foster collaboration among engineers. At e2e.ti.com, you can ask questions, share knowledge, explore ideas and help solve problems with fellow engineers.
    Design Support TI's Design Support Quickly find helpful E2E forums along with design support tools and contact information for technical support.

11.3 Trademarks

SPI, QSPI, MICROWIRE, E2E are trademarks of Texas Instruments.

All other trademarks are the property of their respective owners.

11.4 Electrostatic Discharge Caution

esds-image

These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.

11.5 Glossary

SLYZ022 — TI Glossary.

This glossary lists and explains terms, acronyms, and definitions.