SBAS941A May 2019 – November 2019 AMC1035-Q1
PRODUCTION DATA.
If a full-scale input signal is applied to the AMC1035-Q1 (that is, |VIN| ≥ |VClipping|), the device generates a single one or zero every 128 bits at DOUT, as shown in Figure 43, depending on the actual polarity of the signal being sensed. This feature is also supported with a Manchester coded output and allows full-scale and invalid input signals to be identified as described in the Fail-Safe Output section and can be used for advanced system-level diagnostics.
Figure 43. Overrange Output of the AMC1035-Q1