SLUSEG2D September 2022 – February 2025 BQ25620 , BQ25622
PRODUCTION DATA
After the REGN LDO powers up, the device checks the current capability of the input source. The input source has to meet the following requirements in order to move forward to the next power on steps.
Once these conditions are met, the device proceeds to input source type detection.