SNLS564B December 2017 – January 2024 FPC202
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
If I2C is used as the host-side communication protocol, the maximum number of FPC202 devices which can share a single I2C bus is 14. This allows for controlling up to 28 downstream ports through a single I2C bus.
I2C is an addressed interface. To reduce pin count and simplify integration, the FPC202 has an auto-addressing scheme whereby all FPC202s in a system will take on a unique address without requiring dedicated address pins. This is accomplished by connecting one FPC202’s CTRL4 (ADDR_DONE_N) pin to the subsequent FPC202’s CTRL3 (SET_ADDR_N) pin. The first FPC202 will connect CTRL3 (SET_ADDR_N) to GND, and the final FPC202 will connect CTRL4 (ADDR_DONE_N) to GND, as shown in Figure 7-4.
Figure 7-4 FPC202 Connection Diagram For Unique Addressing in I2C ModeFor I2C host-side control interface implementations, the host controller must first configure each FPC202 device to have a unique address. The CTRL3 (SET_ADDR_N) pin is internally pulled to high logic (regardless of the EN pin status) and the FPC202 device will not respond to any I2C transactions until this pin is pulled low. Once it is driven to low logic, the device will respond to the default I2C 8-bit address (0x1E). A single I2C write to the FPC202 will reassign a new I2C address, and once this is done, the FPC202 will drive low logic with the CTRL4 pin (ADDR_DONE_N) which allows the next FPC202 in the daisy chain to be programmed using the default address. Until this address re-assignment happens, the CTRL4 (ADDR_DONE_N) pin is high-Z.
This scheme allows each FPC202 to take a unique I2C address without any contention on the bus. The addresses may be programmed in any order except for the default 8-bit address (0x1E) which must be assigned to the last device in the daisy chain, or else two FPC202s will respond to 0x1E and there will be bus contention. The state of the CTRL3 (SET_ADDR_N) pin does not matter after the address is reprogrammed (this pin is then used to transfer the LED clock for blinking synchronization). Once the new address is programmed, it becomes fixed and may no longer be changed by a new register write. Only power cycling the device or toggling the EN pin will restore the device to the default re-programmable address.
The I2C address space for FPC202 applications is designed such that each FPC202, each port being controlled, and each logical device address within each port is accessible to the host controller through a unique I2C address. For a system where one or more FPC202s are used to control multiple ports (up to two ports per FPC202), the address of each FPC202 and the address of each each downstream port is shown in Table 7-6.
All FPC202 devices respond to 8-bit I2C address 0x02. This allows the host controller to broadcast write to all FPC202 devices simultaneously.
| FPC202 INSTANCE NUMBER | FPC202 SELF-ADDRESS | PORT 0 | PORT 1 | ||
|---|---|---|---|---|---|
| PRIMARY DEVICE
Default = 0xA0(1) |
SECONDARY DEVICE
Default = 0xA2(1) |
PRIMARY
DEVICE Default = 0xA0(1) |
SECONDARY
DEVICE Default = 0xA2(1) |
||
| ALL | 0x02 | – | – | – | – |
| 0 | 0x04 | 0x20 | 0x22 | 0x28 | 0x2A |
| 1 | 0x06 | 0x30 | 0x32 | 0x38 | 0x3A |
| 2 | 0x08 | 0x40 | 0x42 | 0x48 | 0x4A |
| 3 | 0x0A | 0x50 | 0x52 | 0x58 | 0x5A |
| 4 | 0x0C | 0x60 | 0x62 | 0x68 | 0x6A |
| 5 | 0x0E | 0x70 | 0x72 | 0x78 | 0x7A |
| 6 | 0x10 | 0x80 | 0x82 | 0x88 | 0x8A |
| 7 | 0x12 | 0x90 | 0x92 | 0x98 | 0x9A |
| 8 | 0x14 | 0xA0 | 0xA2 | 0xA8 | 0xAA |
| 9 | 0x16 | 0xB0 | 0xB2 | 0xB8 | 0xBA |
| 10 | 0x18 | 0xC0 | 0xC2 | 0xC8 | 0xCA |
| 11 | 0x1A | 0xD0 | 0xD2 | 0xD8 | 0xDA |
| 12 | 0x1C | 0xE0 | 0xE2 | 0xE8 | 0xEA |
| 13 | 0x1E | 0xF0 | 0xF2 | 0xF8 | 0xFA |
The timing specification for an I2C transaction is described in Figure 7-5.
Figure 7-5 I2C Timing Diagram