SLCS007K September 1973 – March 2017 LM111 , LM211 , LM311
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Validate and test the design implementation to confirm system functionality.
A typical LMx11 application compares a single signal to a reference or two signals against each other. Many users take advantage of the open-drain output to drive the comparison logic output to a logic voltage level to an MCU or logic device. The wide supply range and high voltage capability makes LMx11 optimal for level shifting to a higher or lower voltage.
Figure 13. Zero-Crossing Detector
For this design example, use the parameters listed in Table 1 as the input parameters.
| PARAMETER | MIN | TYP | MAX | UNIT | |
|---|---|---|---|---|---|
| VIN | Input voltage range | –15 | 13 | V | |
| VCC+ | Positive supply voltage | 15 | V | ||
| VCC– | Negative supply voltage | –15 | |||
| IOUT | Output current | 20 | mA | ||
When using LMx11 in a general comparator application, determine the following:
When choosing the input voltage range, consider the input common mode voltage range (VICR). Operation outside of this range can yield incorrect comparisons.
The following list describes the outcomes of some input voltage situations.
Overdrive voltage is the differential voltage produced between the positive and negative inputs of the comparator over the offset voltage (VIO). To make an accurate comparison the Overdrive voltage (VOD) must be higher than the input offset voltage (VIO). Overdrive voltage can also determine the response time of the comparator, with the response time decreasing with increasing overdrive. Figure 14 and Figure 15 show positive and negative response times with respect to overdrive voltage.
Output current is determined by the pullup resistance and pullup voltage. The output current produces a output low voltage (VOL) from the comparator, in which VOL is proportional to the output current. Use Figure 5 to determine VOL based on the output current.
The output current can also effect the transient response.
The load capacitance (CL), pullup resistance (RPULLUP), and equivalent collector-emitter resistance (RCE) levels determine the transient response. Equation 1 approximates the positive response time. Equation 2 approximates the negative response time. RCE can be determine by taking the slope of Figure 5 in the linear region at the desired temperature, or by Equation 3.



where
Figure 14. Output Response for Various Input Overdrives
Figure 15. Output Response for Various Input Overdrives
Figure 16 through Figure 33 show various applications for the LM111, LM211, and LM311 comparators.
Figure 16. 100-kHz Free-Running Multivibrator
Figure 19. TTL Interface With High-Level Logic
Figure 20. Detector for Magnetic Transducer
Figure 22. Comparator and Solenoid Driver
Figure 24. Low-Voltage Adjustable Reference Supply
Figure 21. 100-kHz Crystal Oscillator
Figure 23. Strobing Both Input and Output Stages Simultaneously
Figure 25. Zero-Crossing Detector Driving MOS Logic
Figure 26. Precision Squarer
Figure 27. Digital Transmission Isolator
Figure 28. Positive-Peak Detector
Figure 29. Negative-Peak Detector
Figure 30. Precision Photodiode Comparator
Figure 31. Relay Driver With Strobe
Figure 32. Switching Power Amplifier
Figure 33. Switching Power Amplifiers