SNVS089P July 2000 – September 2026 LM3488
PRODUCTION DATA
The device is set to run as soon as the input voltage crosses above the UVLO set point and at a frequency set according to the FA/SYNC/SD pin pull-down resistor or to run at a frequency set by the waveform applied to the FA/SYNC/SD pin.
If the FA/SYNC/SD pin is pulled high, the LM3488 enters shut-down mode.
If the voltage at the ISEN pin exceeds Vsc, the device enters short-circuit protection mode.