SNOSDI6 October 2026 LMP8640-Q1
PRODUCTION DATA
The input stage of an Analog to Digital converter can be modeled with a resistor and a capacitance to ground. So if the voltage source does not have a low impedance, an error in amplitude measurement occurs. In this case, a buffer is needed to drive the ADC. LMP8640-Q1 and LMP8640HV-Q1 have internal output buffer able to directly drive a capacitive load up to 30 pF, or, the input stage of an ADC. An external low pass RC filter is recommended to be added to the output of LMP8640-Q1 and LMP8640HV-Q1 to reduce the noise and limit the bandwidth of the current sense measurement.
If the supply voltage of LMP8640-Q1 and LMP8640HV-Q1 is higher than the ADC supply voltage, care must be taken to prevent LMP8640-Q1 and LMP8640HV-Q1 output from over-driving the ADC input.
This can be accomplished with a series resistance (which must be present when driving a ADC) and a clamping diode to the ADCs power supply. The diode clamps the ADC input to a safe level. Do not completely rely on a calculated maximum output voltage. Transients or fault conditions outside the normal conditions area can cause the output to swing to a higher than expected voltage.