SNVSBK2 September 2019 LP8733
PRODUCTION DATA.
The auto-increment feature allows writing several consecutive registers within one transmission. Every time an 8-bit word is sent to the LP8733xx, the internal address index counter is incremented by one and the next register is written. Table 6 shows writing sequence to two consecutive registers. The auto-increment feature does not work for read.
MASTER ACTION | START | DEVICE ADDRESS = X | WRITE | REGISTER ADDRESS | DATA | DATA | STOP | ||||
---|---|---|---|---|---|---|---|---|---|---|---|
LP8733xx | ACK | ACK | ACK | ACK |