SBOSA47B February 2026 – November 2026 OPA2591 , OPA591
PRODMIX
The full-power bandwidth curve has been a staple in datasheets for decades. The full-power bandwidth of an op amp provides some indication about where designers can expect slew-induced distortion on a signal of a given amplitude and frequency. The full-power bandwidth curve is generated using Equation 3.
Figure 6-5 shows the full-power bandwidth of the OPAx591. The curve is a good reference for designers that need to achieve high-voltage, high-frequency output swings with little concern for distortion performance. Unfortunately, the curve provides little indication of the true distortion at any given point on the curve. The full-power bandwidth curve is, after all, only a theoretical value and slew-induced distortion appears gradually as the output nears the maximum rate of change. Furthermore, slew-induced distortion is only one of several sources of op-amp distortion. Therefore, the curve is a decent starting point, but not a reliable source for distortion performance.
Figure 6-6 shows the full power bandwidth in terms of total harmonic distortion (THD) performance for the OPAx591. This curve provides a better indication of the level of distortion that a designer can expect for a signal of a given amplitude and frequency. For example, the OPAx591 can achieve approximately −100dB or better of THD at 70VPP up to approximately 1kHz. As a second example, the OPAx591 can achieve approximately −130dB or better of THD at 10VPP up to about 1kHz. As a result of limitations in measurement bandwidth, only 20kHz data are recorded.