SLVS238K August 1999 – September 2023 TL331 , TL331B , TL391B
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Output current is determined by the load/pull-up resistance and logic/pull-up voltage. The output current will produce a output low voltage (VOL) from the comparator. In which VOL is proportional to the output current. Use Figure 6-3 to determine VOL based on the output current.
The output current can also effect the transient response. More is explained in the next section.