SLLSEN7E October 2015 – September 2017 TMDS171
PRODUCTION DATA.
The TMDS171 is a digital video interface (DVI) or high-definition multimedia interface (HDMI) retimer. The TMDS171 supports four TMDS channels, Audio Return Channel (SPDIF_IN/ARC_OUT), Hot Plug Detect, and a Digital Display Control (DDC) interfaces. The TMDS171 supports signaling rates up to 3.4 Gbps to allow for the highest resolutions of 4k2k30p 24 bits per pixel and up to WUXGA 12-bit color depth or 1080p with higher refresh rates. The TMDS171 can automatically configure itself as a re-driver at low data rate (< 1 Gbps) or as a re-timer above this data rate. For passing compliance and reducing system level design issues several features have been included such as TMDS output amplitude adjust using an external resistor on the VSADJ pin and source termination selection control. Device operation and configuration can be programmed by pin strapping or I2C. Four TMDS171s can be used on one I2C bus when I2C_EN enable and device address set by A0/A1.
To reduce active power the TMDS171 supports dual power supply rails of 1.2 V on VDD and 3.3 V on VCC. The TMDS171 supports several methods of power management. It can enter power down mode using three methods; (1) HPD is low; (2) Writing an 1 to register 09h[3]; or (3) de-asserting OE. If using OE, the device must be reprogrammed via I2C if it was originally programmed this way. The SIG_EN pin enables the signal detect circuit that provides an automatic power-management feature during normal operation. When no valid signal is present on the inputs the device enters Stand by mode. By disabling the detect circuit the receiver block is always on. DDC bridge supports 100 Kbps data rate default and 400 kbps adjustable by software.
TMDS171 supports both fixed EQ gain control or adaptive equalization to compensate for different lengths of input cables or board traces. The EQ gain can be software adjusted by I2C control or selection between two fixed values or adaptive equalization by pin strapping EQ_SEL pin. Implementers can use the TX_TERM_CTL pin to change the transmitter termination impedance for better output performance when working in HDMI1.4b or leave it floating. When floating the TMDS171 in conjunction with the rate detect will automatically change its output termination to be compatible with HDMI1.4b requirements.
The TMDS171 supports single ended mode audio return channel. To assist in ease of implementation the TMDS171 supports receive lane swapping and receive polarity swap. When swapping the input lanes IN_CLK and IN_D2 swap and IN_D1 and IN_D0 swap with each other. Swap works in both retimer and redriver mode. Polarity swap will swap the receive pins n and p channel polarity in each lane and is only available during retimer mode. Both lane swap and polarity swap can be implemented at the same time in retimer mode using I2C control.
Two versions of the device are offered to support extended commercial temperature range 0ºC to 85ºC (TMDS171) or industrial operational temperature range from -40ºC to 85ºC (TMDS171I).
When OE is de-asserted, control signal inputs are ignored; the HDMI inputs and outputs are high impedance. It is critical to transition the OE from a low level to high after the VCC supply has reached the minimum recommended operating voltage. This is achieved by a control signal to the OE input, or by an external capacitor connected between OE and GND. To insure the TMDS171 is properly reset, the OE pin must be de-asserted for at least 100 μs before being asserted. When OE is re-asserted the TMDS171 will have to be reprogrammed if it was programmed by I2C and not pin strapping. When implementing the external capacitor, the size of the external capacitor depends on the power up ramp of the VCC supply, where a slower ramp-up results in a larger value external capacitor. Refer to the latest reference schematic for TMDS171; consider approximately 200 nF capacitor as a reasonable first estimate for the size of the external capacitor. Both OE implementations are shown in Figure 21 and Figure 22.
Figure 21. External Capacitor Controlled OE
Figure 22. OE Input from Active controller
TMDS171 starts to operate after the OE signal is properly set after power up timing complete. See Figure 23, Figure 24, Table 1. If OE is held low until VDD and VCC become stable there is no rail sequence requirement.
Figure 24. CDR Timing for TMDS171
TMDS171 incorporates swap function which can set the input lanes in swap mode. The IN_D2 will route to the OUT_CLK position by swapping with IN_CLK. The IN_D1 swaps with IN_D0. The Swap function only changes the input pins. The EQ setup follows the new mapping, see Figure 25. This function can be used with the SWAP/POL pin 1 and control the register 0x09h bit 7 for SWAP enable. The Swap function works in both redriver and retimer mode. The TMDS171 can also swap the input polarity signals. When SWAP/POL is high the n and p pins on each lane will swap. Polarity swap only works when in retimer mode. When this function is enabled and the device is in automatic cross over mode between redriver and retimer modes, care must be taken to avoid losing polarity swap. When the data rate drops to the redriver level, the polarity swap is lost.
| Normal Op | SWAP = L or CSR 0x09h bit 7 is 1'b1 |
|---|---|
| IN_D2 → OUT_D2 | IN_D2 → OUT_CLK |
| IN_D1 → OUT_D1 | IN_D1 → OUT_D0 |
| IN_D0 → OUT_D0 | IN_D0 → OUT_D1 |
| IN_CLK → OUT_CLK | IN_CLK → OUT_D2 |
Figure 25. TMDS171 Swap Function
Standard TMDS terminations are integrated on all TMDS inputs. External terminations are not required. Each input data channel contains an adaptive or fixed equalizer to compensate for Inter-Symbol Interference (ISI) due to cable, connector, and/or board trace losses. The voltage at the TMDS input pins must be limited under the absolute maximum ratings. TMDS input pins have incorporated failsafe circuits. An unused input channel can be externally biased to prevent output oscillation by connecting the N input pin to be grounded through a 1-kΩ resistor and the other pin left open. The input pins can be polarity changed through local I2C register when in retimer mode.
There are two methods for debugging a system to make sure the inputs to the TMDS171 are valid. A TMDS error checker is implemented to provide a rough Bit Error Rate per data lane. This allows the system implementer to determine how the link between the source and TMDS171 is performing on all three data lanes. See CSR BIT FIELD DEFINITIONS – RX PATTERN VERIFIER CONTROL/STATUS register.
If a high error count is evident the TMDS171 has a way to view the general receiver eye quality. A tool is available that uses the I2C link to down load the data that can be plotted for an eye diagram. This is available per data lane. This tool also provides a method to turn on an internal PRBS generator that will transmit a data signal on the data pins. A clock at the proper frequency is required on the IN_CLK pins to generated the expected output data rate.
The equalizer used to clean up inter-symbol interference (ISI) jitter/loss from the bandwidth-limited board traces or cables. TMDS171 supports fixed receiver equalizer and adaptive equalizer by setting the EQ_SEL/A0 pin or through I2C. When EQ_SEL/A0 is high, the EQ gain is fixed to 10 dB and when set low the EQ gain is set to 7.5 dB. TMDS171 operates in adaptive equalizer mode when EQ_SEL/A0 pin is left floating. The EQ gain will be automatically adjusted based on the data rate to compensate for trace or cable loss. Implementers can enable the various EQ settings through local I2C control.
When SIG_EN is enabled, the TMDS looks for a valid TMDS clock signal input. The terminations on the TMDS data lines are connected and the device is fully functional when a valid signal is detected. If no valid TMDS clock signal is detected, the device enters standby mode waiting for a valid signal at the clock input. The internal CDR is shut down and all of the TMDS outputs are in high-Z status. TMDS signal detect circuit can be set as enable by SIG_EN pin or through local I2C control but is default disabled. Designers are recommended to activate this function in normal operation for power saving.
The Audio Return Channel in TMDS171 enables a TV, via a single HDMI cable, to send audio data “upstream” to an A/V receiver or surround audio controller, increasing user flexibility and eliminating the need for any separate S/PDIF audio connection. The TMDS171 supports single mode audio return channel. Implementers can send the S/PDIF signal to SPDIF_IN. The signal from ARC_OUT is sent to HDMI connectors and is passed through the general HDMI cable to audio receiver. By I2C control, customer can disable ARC_OUT by register. Enabled by default after initialization.
Source termination is disabled at data rates < 2 Gbps. When the data rate is between 2 Gbps and 3.4 Gbps, the output signal may be better if the termination value around 150 Ω to 300 Ω depending upon system implementation. TMDS171 supports two different source termination impedances for ease of implementation. Pin 36, TX_TERM_CTL, offers a selection option to choose the output termination impedance value.
A 1% precision resistor, 7.06 kΩ, connected from VSADJ to ground is recommended to allow the differential output swing to comply with TMDS signal levels. The differential output driver provides a typical 10 mA current sink capability, which provides a typical 500 mV voltage drop across a 50 Ω termination resistor.
Figure 27. TMDS Driver and Termination Circuit
In Figure 27, if VCC (TMDS171 supply) and AVCC (sink termination supply) are both powered, the TMDS output signals are high impedance when OE = high. Both supplies being active are the normal operating condition. Again refer to Figure 27, if VCC is on and AVCC is off, the TMDS outputs source a typical 5 mA current through each termination resistor to ground. A total of 33 mW of power is consumed by the terminations independent of the OEB logical selection. When AVCC is powered on, normal operation (OE controls output impedance) is resumed. When the power source of the device is off and the power source to termination is on, the IO(off), output leakage current, specification ensures the leakage current is limited to 45 μA or less. The PRE_SEL pin provides – 2 dB de-emphasis gain, allowing output signal pre-conditioning to offset interconnect losses from the TMDS171 outputs to a TMDS receiver. De-emphasis is recommended to be set at 0 dB while connecting to a receiver through short PCB route. The VOD of the data lanes and clock lane can be adjusted through I2C. See Table 11 for detail. Figure 1 shows the different output voltages based on the different VSADJ settings.
The TMDS171 provides de-emphasis as a way to compensate for ISI loss between the TMDS171 outputs and a TMDS receiver. There are two methods to implement this function. When in pin strapping mode the PRE_SEL pin controls this function. The PRE_SEL pin provides - 2 dB or 0 dB de-emphasis, which allows the output signal pre-conditioning. De-emphasis is recommended to be set at 0-dB while connecting to a receiver through short PCB traces. When pulled to ground through a 65 kΩ resistor - 2 dB can be realized, see Figure 9. When using I2C, reg0Ch[1:0] is used to make these adjustments.
As there are times that true pre-emphasis may be the best solution there are two methods to accomplish this. If pin strapping is being used the best method is to reduce the VSADJ resistor value thus increasing the VOD swing and then pulling the PRE_SEL pin to ground using a 65 kΩ resistor, see Figure 28. If using I2C there are two methods to accomplish this. The first is similar to pin strapping but reducing VSADJ resistor value and then implementing - 2 db de-emphasis through I2C, reg0Ch[1:0] = 01. The second method is to increase the VOD swing by setting reg0Ch[7:5] = 011 and reg0Ch[1:0] = 01 which will accomplish the same pre-emphasis value, see Figure 29. Note: De-emphasis is only implement able during retimer mode. In redriver mode this function is not available.
Figure 28. Pre-emphasis Using Pin Strapping
Figure 29. Pre-emphasis Using I2C
Clock and Data Recovery Circuits (CDR) are used to track, sample and retime the equalized data bit streams. The CDRs are designed with loop bandwidth to minimize the amount of jitter transfer from the video source to the TMDS outputs. Input jitter within the CDR’s PLL bandwidth, < 1 MHz, is transferred to the TMDS outputs. Higher frequency jitter above the CDR loop bandwidth is attenuated, providing a jitter cleaning function to reduce the amount of high frequency jitter from the video source. The retimer is automatically activated at pixel clock above approximately 100 MHz when jitter cleaning is needed for robust operation. The retimer operates at about 100 Mhz – 340 MHz pixel clock (1 – 3.4 Gbps). At pixel clock below about 100 MHz, the TMDS171 automatically bypasses the internal retimer, and operates as a redriver. When the video source changes resolution, the internal retimer starts the acquisition process to determine the input clock frequency and acquire lock to the new data bit streams. During the clock frequency detection period and the retimer acquisition period that last approximately 7 ms, the TMDS drivers can be kept active (default) or programmed to be disabled to avoid sending invalid clock or data to the downstream receiver. The TMDS171 can support retimer mode across the full data rate range of 250 Mbps - 3.4 Gbps by setting DEV_FUNC_MODE bits at reg0Ah[1:0], See Table 9. For compliance testing such as JTOL for 480 Mbps the PLL must be forced to lock.
The TMDS171 can function as a redriver which compensates for ISI channel loss. In this mode, power is reduced as the CDR and PLL are turned off. When in automatic mode, the TMDS171 is in redriver mode for data rates < 1.0 Gbps. By using I2C the device can be put in Redriver mode for the complete data range of 250 Mbps to 3.4 Gbps. This is done by writing a 00 to register 0Ah[1:0]. If the link has excessive random jitter then retimer mode is the best operating mode. If the link has excessive random jitter, the retimer mode is the best operating mode. When in redriver mode, the device compensates for ISI loss only. When in redriver mode compliance is not ensured as skew compensation and retiming functions are disabled. If a significant amount of random jitter is present, the system may not pass compliance at the connector.
The TMDS171 solves sink/source level issues by implementing a master/salve control mode for the DDC bus. When the TMDS171 detects the start condition on the DDC bus from the SDA_SRC/SCL_SRC, it transfers the data or clock signal to the SDA_SNK/SCL_SNK with little propagation delay. When SDA_SNK detects the feedback from the downstream device, the TMDS171 pulls up or pulls down the SDA_SRC bus and delivers the signal to the source.
The DDC link defaults to 100 kbps but can be set to various values including 400 kbps by setting the correct value to address 0Bh through the I2C interface. The DDC lines are 5 V tolerant when the device is powered off. The HPD goes to high impedance when VCC is under low power conditions < 1.5 V.
NOTE
The TMDS171 utilizes clock stretching for DDC transactions. As there are sources and sinks that do not perform this function correctly as system may not work correctly as DDC transactions are incorrectly transmitted/recieved. To overcome this a snoop configuration can be implemented where the SDA/SCL from the source is connected directly to the SDA/SCL sink. The TMDS171 will need its SDA_SNK and SCL_SNK pins connected to this link.
Mode Selection Definition: reg0Ah[7] is the mode select register, see Table 9. This bit lets the receiver know where the device is located in a system for the purpose of centering the AEQ point. The TMDS171 is targeting sink or dock applications so the default value is 1 which centers the EQ at 12 dB to 13 dB, see Table 12. If the TMDS171 is in a source application the value should be changed to a 0 which centers the EQ at 6.5 dB to 7.5 dB.
The TMDS171 local I2C interface is enabled when I2C_EN/PIN is high. The SCL_CTL and SDA_CTL terminals are used for I2C clock and I2C data respectively. The TMDS171 I2C interface conforms to the two-wire serial interface defined by the I2C Bus Specification, Version 2.1 (January 2000), and supports the fast mode transfer up to 400 kbps.
The device address byte is the first byte received following the START condition from the master device. The 7 bit device address for TMDS171 decides by the combination of EQ_SEL/A0 and A1. Table 4 clarifies the TMDS171 target address.
| TMDS171 I2C Device Address | |||||||||
|---|---|---|---|---|---|---|---|---|---|
| A1/A0 | Bit 7 (MSB) | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 (W/R) | HEX |
| 00 | 1 | 0 | 1 | 1 | 1 | 1 | 0 | 0/1 | BC/BD |
| 01 | 1 | 0 | 1 | 1 | 1 | 0 | 1 | 0/1 | BA/BB |
| 10 | 1 | 0 | 1 | 1 | 1 | 0 | 0 | 0/1 | B8/B9 |
| 11 | 1 | 0 | 1 | 1 | 0 | 1 | 1 | 0/1 | B6/B7 |
The typical source application of the TMDS171 is as a retimer in a TV connecting the HDMI input connector and an internal HDMI receiver through flat cables. The register setup can adjust by source side. When TMDS171 used in sink side application, it received data from input connector and transmit to receiver. The local I2C is not 5 V tolerant and only support 3.3 V. Local I2C buses run at 400 kHz supporting fast-mode I2C operation.
The following procedure is followed to write to the TMDS171 I2C registers:
The following procedure is followed to read the TMDS171 I2C registers:
NOTE
Nno sub-addressing is included for the read procedure, and reads start at register offset 00h and continue byte by byte through the registers until the I2C master terminates the read operation.
Refer to Table 4 for TMDS171 local I2C register descriptions. Reads from reserved fields not described return zeros, and writes are ignored.
A table of bit descriptions is typically included for each register description that indicates the bit field name, field description, and the field access tags. The field access tags are described in Table 5.
| ACCESS TAG | NAME | DESCRIPTION |
|---|---|---|
| R | Read | The field shall be read by software |
| W | Write | The field shall be written by software |
| S | Set | The field shall be set by a write of one. Writes of Zero to the field have no effect |
| C | Clear | The field shall be cleared by a write of one. Writes of Zero to the field have no effect |
| u | Update | Hardware may autonomously update this field |
| NA | No Access | Not accessible or not applicable |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R | R | R | R |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:0 | DEVICE_ID | R | 00h ≈ 07h |
These fields return a string of ASCII characters “TMDS171” preceded by one space characters. TMDS171: 0x00 – 0x07 = {- 0x54”T”, 0x4D”M”, 0x44”D”, 0x53”S”, 0x31”1”, 0x37”7”, 0x31”1”, 0x20}, |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 |
| R | R | R | R | R | R | R | R |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:0 | REV _ID | R | 01h | This field identifies the device revision. 0000001– TMDS171 Revision 1 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 |
| R/W/U | R/W/U | R | R/W/U | R/W | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | Lane_SWAP | R/W/U | 1’b0 | This field Swaps the input lanes as per Figure 25. 0 --- Disable (default) No Lane Swap 1 --- enable: Swaps input lanes (Redriver and Retimer Mode) Note: field is loaded from SWAP/POL pin; Writes are ignored when I2C_EN/PIN = 0 |
| 6 | LANE_POLARITY | R/W/U | 1’b0 | Swaps the input Data and Clock lanes polarity. 0 – Disabled: No polarity swap 1 – Swaps the input Data and Clock lane polarity (Retimer Mode Only) Note: field is loaded from SWAP/POL pin; Writes are ignored when I2C_EN/PIN = 0 |
| 5 | Reserved | R | 1’b0 | Reserved |
| 4 | SIG_EN | R/W/U | 1’b0 | This field enable the clock lane activity detect circuitry. 0 – Disable(Default) Clock detector circuit closed and receiver always works in normal operation. 1 – Enable , Clock detector circuit will make receiver automatic enter the standby state when no valid data detect. Note: field is loaded from SIG_EN pin; Writes are ignored when I2C_EN/PIN = 0 |
| 3 | PD_EN | R/W | 1’b0 | 0 – Normal working (default) 1 – Forced Power down by I2C, Lowest Power state |
| 2 | HPD_AUTO_PWRDWN_DISABLE | R/W | 1’b0 | 0 – Automatically enters power down mode based on HPD_SNK (default) 1 – Will not automatically enter power down mode |
| 1:0 | I2C_DR_CTL | R/W | 2’b10 | I2C data rate supported for configuring device. 00 – 5 Kbps 01 – 10 Kbps 10 – 100 Kbps(default) 11 – 400 Kbps (Note: HPD_AUTO_PWRDWN_DISABLE must be set before enabling 400 Kbps mode) |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 1 | 0 | 1 | 1 | 0 | 0 | 0 | 1 |
| R/W | R/W | R/W | R/W | R | W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | Application Mode Selection | R/W | 1’b1 | See Mode Selection
TMDS171 0 – Source 1 – Sink (Default) |
| 6 | HPDSNK_GATE_EN | R/W | 1’b0 | Swaps the input Data and Clock lanes polarity. The field set the HPD_SNK signal pass through to HPD_SRC or not and HPD_SRC whether held in the de-asserted state. 0 – HPD_SNK passed through to the HPD_SRC ( default ) 1 – HPD_SNK will not pass through to the HPD_SRC. |
| 5 | EQ_ADA_EN | R/W | 1’b1 | This field enable the equalizer functioning state; Writes are ignored when I2C_EN/PIN = 0 0 – Fixed EQ 1 – Adaptive EQ (default) |
| 4 | EQ_EN | R/W | 1’b1 | This field enable the Equalizer; Writes are ignored when I2C_EN/PIN = 0 0 -- EQ disable 1 – EQ enable (default) |
| 3 | Reserved | R | 1’b0 | Reserved |
| 2 | APPLY_RXTX_CHANGES | W | 1’b0 | Self-clearing write-only bit. Writing a 1 to this bit will apply new TX_TERM, HDMI_TWPST1, EQ_EN, EQ_ADA_EN, VSWING, Fixed EQ value settings to the clock and data lanes. Writes to the respective registers do not take immediate effect. This bit does not need to be written if I2C configuration occurs while OE or HPD_SNK are low, I2C PD_EN=1 or there is no HDMI clock applied and SIG_EN is high. |
| 1:0 | DEV_FUNC_MODE. | R/W | 2’b01 | This field selects the Device Working Function Mode. 00 – Redriver Mode across full range 250 Mbps – 3.4 Gbps 01 - Automatic Redriver to Retimer Cross Over at 1.0 Gbps (default) 10 - Reserved 11 - Retimer Mode across full range 250 Mbps – 3.4 Gbps When changing crossover point, need to toggle PD_EN or toggle external HPD_SNK. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R/W/U | R/W/U | R/W | R | R |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W/U | R/W/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:5 | VSWING_DATA | R/W | 3’b000 | Data Output Swing Control (Need Design input on what is available) 000 – Vsadj set (default) 001 – Increase by 7% 010 – Increase by 13% 011 – Increase by 18% 100 – Decrease by 30% 101 – Decrease by 22% 110 – Decrease by 15% 111 – Decrease by 7% |
| 4:2 | VSWING_CLK | R/W | 13’b000 | Clock Output Swing Control: Default is set by DR which means standard based swing values but this allows for the swing to be overridden by selecting one of the following values. 000 – Set by Data Rate 001 – Increase by 7% 010 – Increase by 13% 011 – Increase by 18% 100 – Decrease by 30% 101 – Decrease by 22% 110 – Decrease by 15% 111 – Decrease by 7% |
| 1:0 | HDMI_TWPST1[1:0] | R/W/U | 2’b00 | HDMI pre-emphasis FIR post-cursor-1 signed tap weight. 00 – No pre-emphasis 01 – 2 dB pre-emphasis. 10 – Reserved 11 – Reserved Note: Reflects value of PRE_SEL pin; Writes are ignored when I2C_EN/PIN = 0 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 |
| R | R | R/W | R/W | R/W | R/W | R/W | R |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:6 | Reserved | R | 2’b00 | Reserved |
| 5:3 | Data Lane EQ | R/W | 1’b000 | Sets Fixed EQ Values 000 – 0 dB 001 – 4.5 dB 010 – 6.5 dB 011 – 8.5 dB 100 – 10.5 dB 101 – 12 dB 110 – 14 dB 111 – 16.5 dB |
| 2:1 | Clock Lane EQ | R/W | 13’b000 | - Sets Fixed EQ Values. 00 – 0 dB 01 – 1.5 dB 10 – 3 dB 011 – RSVD |
| 0 | Reserved | R | 1’b1 | Reserved |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | PV_SYNC[3:0] | R/W | 4’b0000 | Pattern timing pulse. This field is updated for 8UI once every cycle of the PRBS generator. 1 bit per lane. |
| 3:0 | PV_LD[3:0] | R/W | 4’b0000 | Load pattern-verifier controls into RX lanes. When asserted high, the PV_TO, PV_SEL, PV_LEN, PV_CP20, and PV_CP values are enabled into the corresponding RX lane. These values are then latched and held when PV_LD[n] is subsequently de-asserted low. 1 bit per lane. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/U | R/U | R/U | R/U | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | PV_SYNC[3:0] | R/U | 4’b0000 | Pattern verification mismatch detected. 1 bit per lane. |
| 3:0 | PV_LD[3:0] | R/U | 4’b0000 | Pattern search/training in progress. 1 bit per lane. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/W | R | R/W | R/W | R/W | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | PV_CP20 | R/W | 1’b0 | Customer pattern length 20/16 bits. 0 – 16 bits 1 – 20 bits |
| 6 | Reserved | R | 1’b0 | Reserved |
| 5:3 | PV_LEN[2:0] | R,W | 3’b000 | ]PRBS pattern length 000 – PRBS7 001 – PRBS11 010 – PRBS23 011 – PRBS31 100 – PRBS15 101 – PRBS15 110 – PRBS20 111 – PRBS20 |
| 2:0 | PV_SEL[24:0] | R/W | 3’b000 | Pattern select control 000 – Disabled 001 – PRBS 010 - Clock 011 - Custom 1xx – Timing only mode with sync pulse spacing defined by PV_LEN |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | PV_CP[7:0] | R/W | ‘h00 | Custom pattern data. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | PV_CP[15:8] | R/W | ‘h00 | Custom pattern data. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R/W | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | Reserved | R | 4’b0000 | Reserved |
| 3:0 | PV_CP[19:16] | R/W | 4’b0000 | Custom pattern data. Used when PV_CP20 = 1’b1. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:3 | Reserved | R | 5’b00000 | Reserved |
| 2:0 | PV_THR[2:0] | R/W | 3’b000 | Pattern-verifier retain threshold. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R/S/U | R/S/U | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | DESKEW_CMPLT | R | 1’b0 | Indicates that TMDS lane deskew has completed when high. |
| 6:5 | Reserved | R | 2’b00 | Reserved |
| 4 | BERT_CLR | R/S/U | 1’b0 | Clear BERT counter (on rising edge). |
| 3 | TST_INTQ_CLR | R/S/U | 1’b0 | Clear latched interrupt flag. |
| 2:0 | TST_SEL[2:0] | R/W | 3’b000 | Test interrupt source select. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/W | R/W | R/W | R/W | R | R/W | R/W | R/W |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | PV_DP_EN[3:0] | R/W | 4’b0000 | Enable datapath verified based on DP_TST_SEL, 1 bit per lane |
| 3 | Reserved | R | 1’b0 | Reserved |
| 2:0 | DP_TST_SEL[2:0] | R/W | 3’b000 | Selects pattern reported by BERT_CNT[11:0], TST_INT[0] and TST_INTQ[0] and PV_DP_EN is non-zero. 000 – TMDS disparity or data errors 001 – FIFO errors 010 – FIFO overflow errors 011 – FIFO underflow errors 100 – TMDS deskew status 101,110,111 – Reserved. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/U | R/U | R/U | R/U | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | TST_INTQ[3:0] | R/U | 4’b0000 | Latched interrupt flag. 1 bit per lane |
| 3:0 | RTST_INT[3:0] | R/U | 4’b0000 | Test interrupt flag. 1 bit per lane. |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/U | R/U | R/U | R/U | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:0 | BERT_CNT[7:0] | R/U | ‘h00 | BERT error count. Lane 0 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | Reserved | R | 4’b0000 | Reserved |
| 3:0 | BERT_CNT[11:8] | R/U | 4’b0000 | BERT error count. Lane 0 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/U | R/U | R/U | R/U | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:0 | BERT_CNT[19:12]. | R/U | ‘h00 | BERT error count. Lane 1 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | Reserved | R | 4’b0000 | Reserved |
| 3:0 | BERT_CNT[23:20] | R/U | 4’b0000 | BERT error count. Lane 1 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/U | R/U | R/U | R/U | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:0 | BERT_CNT[31:24] | R/U | ‘h00 | BERT error count. Lane 2 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | Reserved | R | 4’b0000 | Reserved |
| 3:0 | BERT_CNT[35:32] | R/U | 4’b0000 | BERT error count. Lane 2 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R/U | R/U | R/U | R/U | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:0 | BERT_CNT[19:12] | R/U | ’h00 | BERT error count. Lane 3 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R | R | R/U | R/U | R/U | R/U |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7:4 | Reserved | R | 4’b0000 | Reserved |
| 3:0 | BERT_CNT[23:20] | R/U | 4’b0000 | BERT error count. Lane 3 |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| R | R | R/W | R/W | R | R | R | R |
| LEGEND: R/W = Read/Write; R = Read only; -n = value after reset, S= Set, U = autonomously update |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 7 | PWR_DWN_STATUS | R | 1’b0 | Power Down Status Bit. 0 = Normal Operation (default) 1 = Device in Power Down Mode |
| 6 | STB_STATUS | R | 1’b0 | Standby Status Bit 0 = Normal Operation (default) 1 = Device in Standby Mode |
| 5:0 | Reserved | R | 6’b000000 | Reserved |