SLVSBL3D November 2012 – July 2021
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The maximum IC junction temperature should be restricted to 125°C under normal operating conditions. To calculate the maximum allowable dissipation, PD(max) for a given output current and ambient temperature, use the following equation as a guideline:
where
The power dissipated by the device depends on the RON of the device at a given VIN. To calculate the amount of power being dissipated by the device, use the following equation:
where
The result from Equation 2 should always be less than or equal to the result from Equation 1.