SLVSI78B January 2025 – December 2025 TPS542021 , TPS542025
PRODUCTION DATA
Consider three primary factors when selecting the value of the output capacitor. The output capacitor determines the modulator pole, the output voltage ripple, and how the regulator responds to a large change in load current. The output capacitance must be selected based on the more stringent of these three criteria.
The desired response to a large change in the load current is the first criterion. The output capacitor must supply the load with current when the regulator cannot. This situation occurs if the desired hold-up times are present for the regulator. In this case, the output capacitor must hold the output voltage above a certain level for a specified amount of time after the input power is removed. The regulator is also temporarily unable to supply sufficient output current if a large, fast increase occurs affecting the current requirements of the load, such as a transition from no load to full load. The regulator typically requires two or more clock cycles for the control loop to notice the change in load current and output voltage and to adjust the duty cycle to react to the change. The output capacitor must be sized to supply the extra current to the load until the control loop responds to the load change. The output capacitance must be large enough to supply the difference in current for two clock cycles while only allowing a tolerable amount of drop in the output voltage. Use the following equation to calculate the minimum required output capacitance.
where:
For this example, the transient load response is specified as a 5% change in the output voltage, VOUT, for a load step of 1.5A. For this example, ΔIOUT = 1.5A and ΔVOUT = 0.05 × 5 = 0.25V. Using these values results in a minimum capacitance of 24μF. This value does not consider the ESR of the output capacitor in the output voltage change. For ceramic capacitors, the ESR is typically small enough to ignore in this calculation.
Equation 12 calculates the minimum output capacitance required to meet the output voltage ripple specification. In this case, the maximum output voltage ripple is 30mV. Under this requirement, Equation 12 yields 4.56μF.
where:
Use Equation 13 to calculate the maximum ESR an output capacitor can have to meet the output-voltage ripple specification. Equation 13 indicates the ESR must be less than 54.8mΩ. In this case, the ESR of the ceramic capacitor is much smaller than 54.8mΩ.
The output capacitor can affect the crossover frequency ƒo. Considering to the loop stability and effect of the internal parasitic parameters, choose the crossover frequency less than 40kHz without considering the feed forward capacitor. A simple estimation for the crossover frequency without feed forward capacitor C6 is shown in Equation 14, assuming COUT has small ESR.
Additional capacitance deratings for aging, temperature, and DC bias must be considered, which increases this minimum value. For this example, two 22uF 25V, X7R ceramic capacitors are used. Capacitors generally have limits to the amount of ripple current the capacitors can handle without failing or producing excess heat. An output capacitor that can support the inductor ripple current must be specified. Some capacitor data sheets specify the RMS value of the maximum ripple current. Use Equation 15 to calculate the RMS ripple current that the output capacitor must support. For this application, Equation 15 yields 79mA for each capacitor.