SLVS258B November   1999  – December 2016 TPS60130 , TPS60131 , TPS60132 , TPS60133

PRODUCTION DATA.  

  1. 1 Features
  2. 2 Applications
  3. 3 Description
  4. 4 Revision History
  5. 5 Device Options
  6. 6 Pin Configuration and Functions
  7. 7 Specifications
    1. 7.1 Absolute Maximum Ratings
    2. 7.2 ESD Ratings
    3. 7.3 Recommended Operating Conditions
    4. 7.4 Thermal Information
    5. 7.5 Electrical Characteristics
    6. 7.6 Dissipation Ratings
    7. 7.7 Typical Characteristics
  8. 8 Parameter Measurement Information
  9. 9 Detailed Description
    1. 9.1 Overview
    2. 9.2 Functional Block Diagram
    3. 9.3 Feature Description
      1. 9.3.1 Operating Principle
      2. 9.3.2 Adaptive Mode Switching
      3. 9.3.3 Pulse-Skip Mode
      4. 9.3.4 Start-Up Procedure
      5. 9.3.5 Shutdown
      6. 9.3.6 Undervoltage Lockout
      7. 9.3.7 Low Battery Detector (TPS60130 and TPS60132)
      8. 9.3.8 Power Good Detector (TPS60131 and TPS60133)
  10. 10Application and Implementation
    1. 10.1 Application Information
    2. 10.2 Typical Applications
      1. 10.2.1 Paralleling of Two TPS6013x to Deliver 600-mA Total Output Current
        1. 10.2.1.1 Design Requirements
        2. 10.2.1.2 Detailed Design Procedure
          1. 10.2.1.2.1 Capacitor Selection
        3. 10.2.1.3 Application Curves
      2. 10.2.2 TPS6013x Operated With Ultra-Low Quiescent Current
        1. 10.2.2.1 Design Requirements
      3. 10.2.3 Regulated Discharge of the Output Capacitors After Disabling of the TPS6013x
        1. 10.2.3.1 Design Requirements
  11. 11Power Supply Recommendations
  12. 12Layout
    1. 12.1 Layout Guidelines
    2. 12.2 Layout Example
    3. 12.3 Power Dissipation
  13. 13Device and Documentation Support
    1. 13.1 Documentation Support
      1. 13.1.1 Related Documentation
    2. 13.2 Related Links
    3. 13.3 Receiving Notification of Documentation Updates
    4. 13.4 Community Resources
    5. 13.5 Trademarks
    6. 13.6 Electrostatic Discharge Caution
    7. 13.7 Glossary
  14. 14Mechanical, Packaging, and Orderable Information

Package Options

Mechanical Data (Package|Pins)
Thermal pad, mechanical data (Package|Pins)
Orderable Information

Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

Application Information

The TPS6013x charge pumps provide a regulated 5-V output from a 2.7-V to 5.4-V input. They deliver a maximum load current of 300 mA or 150 mA (respectively).

Typical Applications

Paralleling of Two TPS6013x to Deliver 600-mA Total Output Current

Two TPS60130x devices can be connected in parallel to yield higher load currents. The circuit of Figure 23 can deliver up to 600 mA at an output voltage of 5 V.

TPS60130 TPS60131 TPS60132 TPS60133 bd_paralleling_two_tps6013x_charge_pumps_slvs258a.gif Figure 23. Paralleling of Two TPS6013x Charge Pumps

Design Requirements

The device operates over an input voltage range from 2.7 V to 5.4 V.

Detailed Design Procedure

The devices can share the output capacitors, but each one requires its own transfer capacitors and input capacitor. If both a TPS60130 and a TPS60131 are used, it is possible to monitor the battery voltage with the TPS60130 using the low battery comparator function and to supervise the output voltage with the TPS60131 using the Power Good comparator. Make the layout of the charge pumps as similar as possible, and position the output capacitor the same distance from both devices.

Capacitor Selection

The TPS6013x charge pump require only four external capacitors as shown in the basic application circuit. Their capacitance values and types are closely linked to the output current and output noise and ripple requirements. For lowest noise and ripple, low ESR (<0.1 Ω) capacitors must be used for input and output capacitors.

The input capacitor improves system efficiency by reducing the input impedance. It also stabilizes the input current of the power source. The input capacitor must be chosen according to the power supply used and the distance from power source to the converter IC. The input capacitor also has an impact on the output voltage ripple. The lower the ESR of the input capacitor Ci, the lower is the output ripple. TI recommends Ci be about two to four times as large as C(xF).

The output capacitor Co can be selected from 5-times to 50-times larger than C(xF), depending on the ripple tolerance. The larger Co, the lower is the output voltage ripple. Ci and Co can be either ceramic or low-ESR tantalum; aluminum capacitors are not recommended.

Generally, the flying capacitors C(xF) is the smallest. Only ceramic capacitors are recommended, due to their low ESR and because they retain their capacitance at the switching frequency. Because the device regulates the output voltage using the pulse-skip technique, a larger flying capacitor leads to a higher output voltage ripple if the size of the output capacitor is not increased. Be aware that, depending on the material used to manufacture them, ceramic capacitors might lose their capacitance over temperature. Ceramic capacitors of type X7R or X5R material keep their capacitance over temperature and voltage, whereas Z5U or Y5V-type capacitors decrease in capacitance. Table 5 lists recommended capacitor values.

Table 5. Recommended Capacitor Values

PART VI (V) IO (mA) Ci (µF) CxF
CERAMIC (X7R)
Co (µF) VPP(TYP) (V)
TANTALUM CERAMIC (X7R) TANTALUM CERAMIC (X7R)
TPS60130,
TPS60131
3.6 225 — 10 2.2 22 4.7 90
— — 22 60
TPS60132,
TPS60133
3.6 300 — 10 2.2 33 4.7 120
— — 22 and 10
in parallel
45
75 — 4.7 1 — 10 —
150 4.7 2.2 15 22 100
— 4.7 — 22 90

The TPS6013x devices are charge pumps that regulate the output voltage using pulse-skip regulation mode. The output voltage ripple is therefore dependent on the values and the ESR of the input, output and flying capacitors. The only possibility to reduce the output voltage ripple is to choose the appropriate capacitors. The lowest output voltage ripple can be achieved using ceramic capacitors because of their low ESR and their frequency characteristic.

Ceramic capacitors typically have an ESR that is more than 10 times lower than tantalum capacitors and they retain their capacitance at frequencies more than 10 times higher than tantalum. Many different tantalum capacitors act as an inductance for frequencies higher than 200 kHz. This behavior increases the output voltage ripple. Therefore, the best choice for a minimized ripple is the ceramic capacitor. For applications that do not require a higher performance in output voltage ripple, tantalum capacitors with a low ESR are a possibility for input and output capacitor, but a ceramic capacitor must be connected in parallel. Be aware that the ESR of tantalum capacitors is indirectly proportional to the physical size of the capacitor.

Table 5 is a good starting point for choosing the capacitors. If the output voltage ripple is too high for the application, it can be improved by selecting the appropriate capacitors. The first step is to increase the capacitance at the output. If the ripple is still too high, the second step would be to increase the capacitance at the input.

For the TPS60130 and TPS60131, the smallest board space can be achieved using Sprague’s 595D-series tantalum capacitors for input and output. However, high-capacitance ceramic capacitors become competitive in package size soon.

The smallest size for the lower-current devices TPS60132 and TPS60133 can be achieved using the suggested ceramic capacitors.

Table 6 lists the manufacturers of recommended capacitors. In most applications, surface-mount tantalum capacitors is the right choice. However, ceramic capacitors provide the lowest output voltage ripple due to their typically lower ESR.

Table 6. Recommended Capacitors(1)

MANUFACTURER PART NUMBER CAPACITANCE CASE SIZE TYPE
Taiyo Yuden LMK212BJ105KG−T 1 µF 0805 Ceramic
LMK212BJ225MG−T 2.2 µF 0805 Ceramic
LMK316BJ475KL−T 4.7 µF 1206 Ceramic
LMK325BJ106MN−T 10 µF 1210 Ceramic
LMK432BJ226MM−T 22 µF 1812 Ceramic
AVX 0805ZC105KAT2A 1 µF 0805 Ceramic
1206ZC225KAT2A 2.2 µF 1206 Ceramic
TPSC475035R0600 4.7 µF Case C Tantalum
TPSC156025R0500 10 µF Case C Tantalum
TPSC336010R0375 22 µF Case C Tantalum
Sprague 595D156X0016B2T 15 µF Case B Tantalum
595D226X0016B2T 22 µF Case B Tantalum
595D336X0016B2T 33 µF Case B Tantalum
595D336X0016C2T 33 µF Case C Tantalum
Kemet T494C156K010AS 15 µF Case C Tantalum
T494C226K010AS 22 µF Case C Tantalum
T494C336K010AS 33 µF Case C Tantalum
Case code compatibility with EIA 535BAAC and CECC30801 molded chips.

Application Curves

TPS60130 TPS60131 TPS60132 TPS60133 graph_13_SLVS258A.gif
Figure 24. Output Voltage Ripple vs Time
TPS60130 TPS60131 TPS60132 TPS60133 graph_14_SLVS258A.gif
Figure 25. Output Voltage Ripple vs Time
TPS60130 TPS60131 TPS60132 TPS60133 graph_15_SLVS258A.gif
Figure 26. Output Voltage Ripple vs Time
TPS60130 TPS60131 TPS60132 TPS60133 graph_18_SLVS258A.gif
Figure 28. Load Transient Response
TPS60130 TPS60131 TPS60132 TPS60133 graph_20_SLVS258A.gif
Figure 30. Output Voltage vs Time (Start-Up Timing)
TPS60130 TPS60131 TPS60132 TPS60133 graph_16_SLVS258A.gif
Figure 27. Output Voltage Ripple Amplitude
vs Input Voltage
TPS60130 TPS60131 TPS60132 TPS60133 graph_19_SLVS258A.gif
Figure 29. Line Transient Response

TPS6013x Operated With Ultra-Low Quiescent Current

Because the output of the TPS6013x is isolated from the input when the devices are disabled, and because the internal resistive divider is disconnected in shutdown, an ultra-low quiescent current mode can be implemented. In this mode, the output voltage is sustained because the converter is periodically enabled to refresh the output capacitor. The necessary external control signal that is applied to the ENABLE-pin is generated from a microcontroller. For a necessary supply current for the system of 1 mA and a minimum supply voltage of 4.5 V with a 33-µF output capacitor, the refresh has to be done after 9 ms. Longer refresh periods can be achieved with a larger output capacitor.

TPS60130 TPS60131 TPS60132 TPS60133 bd_tps60132_ultra_low_quiescent_current_mode_slvs258A.gif Figure 31. TPS60132 in Ultra-Low Quiescent Current Mode

Design Requirements

The device operates over an input voltage range from 2.7 V to 5.4 V.

Regulated Discharge of the Output Capacitors After Disabling of the TPS6013x

During shutdown of the charge pump TPS6013x the output is isolated from the input. Therefore, the discharging of the output capacitor depends on the load and on the leakage current of the capacitor. In certain applications it is necessary to completely remove the supply voltage from the load in shutdown mode. That means the output capacitor of the charge pump has to be actively discharged when the charge pump is disabled. Figure 5 shows one solution to this problem.

TPS60130 TPS60131 TPS60132 TPS60133 bd_regulated_discharge_output_capacitor_slvs258a.gif Figure 32. Block Diagram of the Regulated Discharge of the Output Capacitor

Design Requirements

The device operates over an input voltage range from 2.7 V to 5.4 V. TI's SN74AHC1G04 and BSS138 is required.