SLVSEK3 March 2018 TPS62243-Q1 , TPS62244-Q1
PRODUCTION DATA.
The inductor value has a direct effect on the ripple current. The selected inductor must be rated for its DC resistance and saturation current (Table 3). The inductor ripple current (ΔIL) decreases with higher inductance and increases with higher VI or VO.
The inductor selection also has an impact on the output voltage ripple in the PFM mode. Higher inductor values lead to lower-output voltage ripple and higher PFM frequency, and lower inductor values lead to a higher-output voltage ripple with lower PFM frequency.
Equation 2 calculates the maximum inductor current in PWM mode under static load conditions. The saturation current of the inductor should be rated higher than the maximum inductor current as calculated with Equation 3. This is the recommendation because during heavy-load transients the inductor current rises above the calculated value.


where
A more conservative approach is to select the inductor current rating just for the maximum switch current limit ILIMF of the converter.
Accepting larger values of ripple current allows the use of low inductance values, but results in higher output voltage ripple, greater core losses, and lower output current capability.
The total losses of the coil strongly impact the efficiency of the DC-DC conversion and consist of both the losses in the DC resistance (R(DC)) and the following frequency-dependent components:
| INDUCTANCE (μH) | DIMENSIONS (mm) | PART NUMBER | MANUFACTURER(1) |
|---|---|---|---|
| 2 | 2.5 × 2 × 1 | MIPS2520D2R2 | FDK |
| 2 | 2.5 × 2 × 1.2 | MIPSA2520D2R2 | FDK |
| 2.2 | 2.5 × 2 × 1 | KSLI-252010AG2R2 | Hitachi Metals |
| 2.2 | 2.5 × 2 × 1.2 | LQM2HPN2R2MJ0L | Murata |
| 2.2 | 3 × 3 × 1.4 | LPS3015 | Coilcraft |