SBVS220C March 2013 – October 2026 TPS7A37
PRODUCTION DATA
The NMOS pass element of the TPS7A37 provides inherent protection against current flow from the output of the regulator to the input when the gate of the pass device is pulled low. To verify that all charge is removed from the gate of the pass element, the EN pin must be driven low before the input voltage is removed. If this is not done, the pass element can be left on because of stored charge on the gate.
After the EN pin is driven low, no bias voltage is needed on any pin for reverse current blocking. Note that reverse current is specified as the current flowing out of the IN pin because of voltage applied on the OUT pin. There is additional current flowing into the OUT pin as a result of the 80kΩ internal resistor divider to ground (see Figure 6-1 and Figure 6-2).
For the TPS7A3701, reverse current can flow when VFB is more than 1.0V above VIN.