SNOSDH4C June 2024 – April 2025 TPS7H6005-SEP , TPS7H6005-SP , TPS7H6015-SEP , TPS7H6015-SP , TPS7H6025-SEP , TPS7H6025-SP
PRODMIX
Refer to the PDF data sheet for device specific package drawings
Gate drive devices such as the TPS7H6005 have several different components that comprise the power losses. The quiescent power losses PQCcan be determined using Equation 21 :
where:
Leakage current power losses PBG can be calculated using Equation 22:
where:
There are losses that occur within the driver due to the charging and discharging of the GaN FET gate charge. To determine these, first calculate PGATE as:
This loss is actually distributed amongst the resistances in the gate driver loop, which includes the driver, the gate resistances and the GaN FET. The power dissipated within the TPS7H6005 for both turn-on and turn-off can be calculated:
In this instance, the high-side and low-side losses are the same:
Finally, the PGATE losses within the driver can be found:
There is also a component of power consumption associated with the operating current of the driver, which is specified at no-load and frequency dependent. These can be approximated using the operating current parameters in the Specifications section:
where: