SLUSG04 March   2025 UC2842L , UC2843L , UC2844L , UC2845L

PRODUCTION DATA  

  1.   1
  2. Features
  3. Applications
  4. Description
  5. Device Comparison
  6. Pin Configuration and Functions
  7. Specifications
    1. 6.1 Absolute Maximum Ratings
    2. 6.2 ESD Ratings
    3. 6.3 Recommended Operating Conditions
    4. 6.4 Thermal Information
    5. 6.5 Electrical Characteristics
    6. 6.6 Typical Characteristics
  8. Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Pulse-by-Pulse Current Limiting
      2. 7.3.2 Current Sense Circuit
      3. 7.3.3 Error Amplifier Configuration
      4. 7.3.4 Undervoltage Lockout
      5. 7.3.5 Oscillator
    4. 7.4 Device Functional Modes
      1. 7.4.1 Normal Operation
      2. 7.4.2 Undervoltage Lockout (UVLO) Start-Up
      3. 7.4.3 UVLO Turnoff Mode
  9. Application and Implementation
    1. 8.1 Application Information
    2. 8.2 Typical Application
      1. 8.2.1 Design Requirements
      2. 8.2.2 Detailed Design Procedure
        1. 8.2.2.1 Custom Design With WEBENCH® Tools
        2. 8.2.2.2 UC2842L Design Procedure
      3. 8.2.3 Application Curves
    3. 8.3 Power Supply Recommendations
    4. 8.4 Layout
      1. 8.4.1 Layout Guidelines
      2. 8.4.2 Layout Example
  10. Device and Documentation Support
    1. 9.1 Device Support
      1. 9.1.1 Device Nomenclature
    2. 9.2 Documentation Support
      1. 9.2.1 Related Documentation
    3. 9.3 Receiving Notification of Documentation Updates
    4. 9.4 Support Resources
    5. 9.5 Trademarks
    6. 9.6 Electrostatic Discharge Caution
    7. 9.7 Glossary
  11. 10Revision History
  12. 11Mechanical, Packaging, and Orderable Information

Package Options

Mechanical Data (Package|Pins)
Thermal pad, mechanical data (Package|Pins)
Orderable Information

UC2842L Design Procedure

This application design procedure shows how to setup and use the UC2842L peak current mode controller in an offline flyback converter, with universal input to a 12-V, 48-W regulated output.

Setting up and designing with the UC2842L peak current mode controller in a continuous mode flyback application requires knowing some things about the power stage. First, calculate the required input bulk capacitance (CIN) based on output power level (POUT), efficiency (ƞ), minimum input voltage (VIN(min)), line frequency (fLINE) and minimum bulk voltage. For this design example let VBULK(min) = 95V.

Equation 2. UC2842L UC2843L UC2844L UC2845L
Equation 3. UC2842L UC2843L UC2844L UC2845L

The output capacitor (COUT) is sized so the output voltage does not droop more than 10% during a large-signal transient response. The voltage-loop crossover frequency (fC) is estimated to be 2.5kHz at this point in the design.

Equation 4. UC2842L UC2843L UC2844L UC2845L

The COUT selected for the design is a 2200-µF capacitor, with an equivalent series resistance (ESR) of 45mΩ.

Next calculate the maximum primary to secondary turns ratio (NPS) of the transformer, based on the minimum input voltage and output voltage.

Equation 5. UC2842L UC2843L UC2844L UC2845L

Next calculate the auxiliary to secondary turns ratio (NAS) of the transformer, based on the output voltage and the bias voltage of the UC2842A.

Equation 6. UC2842L UC2843L UC2844L UC2845L

Once the transformer turns ratios have been determined, the minimum primary magnetizing inductance (LPM) of the transformer can be calculated based on minimum bulk voltage, Duty Cycle (D), reflected output current and efficiency. The transformer used in this design has an LPM of 1.7mH, NPS = 10, and a NAS = 1, fsw = 100kHz

Equation 7. UC2842L UC2843L UC2844L UC2845L
Equation 8. UC2842L UC2843L UC2844L UC2845L

After the transformer has been selected, the primary peak current (ILpPK) of the transformer can be calculated based on the primary magnetizing inductance ripple (ILPM) and the reflected output current across the transformer.

Equation 9. UC2842L UC2843L UC2844L UC2845L
Equation 10. UC2842L UC2843L UC2844L UC2845L

Once the primary peak current has been calculated the current sense resistor (RCS) can be selected.

Equation 11. UC2842L UC2843L UC2844L UC2845L

Resistors RS1 and RS2 are used to set the slope compensation of the design. Capacitor CS1 is a DC blocking capacitor, and pull-up resistor RP is used to provide some offset to the current sense signal for noise immunity. RP and RS2 were preselected to add a DC offset of 50mV to the current sense signal.

RS1 is selected to set the slope compensation to one-half of the ripple current down slope of the flyback inductor. This can be accomplished by calculating the secondary magnetizing inductance (LSM) and using the following calculation for RS1. The 1.7V in the RS1 equation is the peak-to-peak ripple voltage amplitude of the oscillator.

Equation 12. UC2842L UC2843L UC2844L UC2845L

where

  • UC2842L UC2843L UC2844L UC2845L

Resistors RI and RK are selected to the output reference and can be calculated by preselecting a value for RK and knowing the TL431 reference voltage (VTL431REF). After choosing 2.49 kΩ for RK, RI is calculated and a standard resistor value of 9.53kΩ is chosen for this resistor.

Equation 13. UC2842L UC2843L UC2844L UC2845L

This design using the UC2842L controller has an interesting control loop with many components. GOPTO(f) is the approximate transfer function across the opto isolator in the design. The pole frequency of the opto isolator is represented by fP. The opto isolator used in this design has a current transfer ratio of 1 and pole frequency of roughly 5kHz. See Figure 8-1 for component placement and node voltages. The voltage loop (fC) must cross-over less than the opto isolator pole for simplified compensation.

Equation 14. UC2842L UC2843L UC2844L UC2845L
Equation 15. UC2842L UC2843L UC2844L UC2845L
Equation 16. UC2842L UC2843L UC2844L UC2845L

GBC(f) is an estimate of the transfer function from the output of the opto isolator to the PWM’s control voltage .

Equation 17. UC2842L UC2843L UC2844L UC2845L

The duty cycle varies with the bulk input voltage (VBULK). VBULK varies from 95V to 375V during normal operation. This causes the duty cycle to vary from 24% to 56%.

Equation 18. UC2842L UC2843L UC2844L UC2845L

GCO(f) is an estimate of the control (VC) to output transfer function, where variable Q is the quality factor.

Equation 19. UC2842L UC2843L UC2844L UC2845L

The quality factor (Q) is defined by the primary magnetizing inductance change in voltage (SN) as a function of duty cycle; as well as, the added slope compensation (SE).

Equation 20. UC2842L UC2843L UC2844L UC2845L
Equation 21. UC2842L UC2843L UC2844L UC2845L
Equation 22. UC2842L UC2843L UC2844L UC2845L

To ensure that the voltage loop is stable, the crossover frequency must be less than one half of the right-half-plane zero frequency (fRHPZ) of the flyback converter. The right-half-plane zero frequency at the minimum bulk voltage would be roughly 9.8kHz. For this design example the target crossover of the voltage loop is at 1kHz. The actual fC may be higher or lower than the target.

Equation 23. UC2842L UC2843L UC2844L UC2845L
Equation 24. UC2842L UC2843L UC2844L UC2845L

The DC gain of GCO(f) moves with the bulk input voltage. Resistor RZ is selected to crossover the voltage loop when input to the converter is at VBULK(min) and to crossover at 1/5th the maximum crossover frequency.

Equation 25. UC2842L UC2843L UC2844L UC2845L

Capacitor CZ is selected to add 45° of phase margin at voltage loop crossover. For this design example a 6.8-nF capacitor was used.

Equation 26. UC2842L UC2843L UC2844L UC2845L

Capacitor CP is selected to attenuate the high frequency gain of the control loop.

Equation 27. UC2842L UC2843L UC2844L UC2845L

GC(f) is the estimated transfer function of the TL431 compensation.

Equation 28. UC2842L UC2843L UC2844L UC2845L

TV(f) is the estimated theoretical transfer function of the close-loop gain of the system. The feedback loop response may be different in the actual circuit and may have to be adjusted with a network analyzer to meet actual circuit performance and reliability. The feedback loop response must be evaluated over worse case variations in design parameters.

Equation 29. UC2842L UC2843L UC2844L UC2845L

For this application example, this design technique generated a theoretical feedback loop (TV(f)) crossover at 1kHz with roughly 55° of phase margin at a minimum input bulk voltage of 95V. The theoretical voltage loop at high-line crossed over at 2.7kHz with a phase margin of 72°. See Figure 8-2 and Figure 8-3. TV(f) must be evaluated with a network analyzer and adjust the loop compensation as necessary based on the actual circuitry behavior. Also conduct transient testing to ensure that the device remains stable.