SLUSFA0 September 2023 UCC21738-Q1
PRODUCTION DATA
Figure 9-1 shows the typical application of a half bridge using two UCC21738-Q1 isolated gate drivers. The half bridge is a basic element in various power electronics applications, such as a traction inverter in a HEV/EV to convert DC current of the electric battery of the vehicle to AC current to drive the electric motor in the propulsion system. The topology can also be used in motor drive applications to control the operating speed and torque of the AC motors.