SLUSFX8 September 2026 UCC218302-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The UCC218302-Q1 implements a fast overcurrent and short-circuit protection feature to protect the power semiconductor device from catastrophic breakdown during a fault. The DESAT pin threshold, VDESATTH, is with respect to COM, the source or emitter of the power semiconductor device. When the driver is in the off state, an internal MOSFET pulls down the DESAT pin to prevent DESAT from false triggering. When the driver is in the on state, an internal current source activates to charge an external capacitor. The UCC218302-Q1 features an internal leading edge blanking time after OUTHx switches to the on state to avoid false triggers from noise during the switching transient. During the leading edge blanking time period, the DESAT pin is pulled-down by the internal pulldown MOSFET. When the driver turns off, the internal pulldown MOSFET discharges the voltage of the DESAT pin. Figure 6-9 shows a simplified block diagram of the DESAT circuit. Figure 6-10 shows timing diagrams showing a DESAT fault, soft shutdown, fault reporting, and fault reset.