JAJSSA6 December 2023 BQ25960H
PRODUCTION DATA
The system will have a specific battery charging profile that is unique due to the switched cap architecture. The charging will be controlled by the main charger such as the BQ2561x or BQ2589x until ystem voltage reaches minimum system regulation voltage VSYSMIN. Once the battery voltage reaches VSYSMIN (3.5 V), the adapter can negotiate for a higher bus voltage, enable BQ25960H charging, and regulate the current on VBUS to charge the battery. In the CC phase, the protection in BQ25960H will not regulate the battery voltage, but will provide feedback to the system to increase and decrease current as needed, as well as disable the blocking and switching FETs if the voltage is exceeded. Once the CV point is reached, the BQ25960H will provide feedback to the adapter to reduce the current, effectively tapering the current until a point where the main charger takes over again. The BQ25960H can operate as long as input current is above the BUSUCP threshold.