JAJSK38 july 2021 BQ51013B-Q1
PRODUCTION DATA
The BQ51013B-Q1 device provides two identical, integrated communication FETs which are connected to the pins COMM1 and COMM2. These FETs are used for modulating the secondary load current which allows the BQ51013B-Q1 to communicate error control and configuration information to the transmitter. Figure 9-10 shows how the COMMx pins can be used for resistive load modulation. Each COMMx pin can handle at most a 24-Ω communication resistor. Therefore, if a COMMx resistor between 12 Ω and 24 Ω is required, COMM1 and COMM2 pins must be connected in parallel. The BQ51013B-Q1 device does not support a COMMx resistor less than 12 Ω.
In addition to resistive load modulation, the BQ51013B-Q1 is also capable of capacitive load modulation as shown in Figure 9-11. In this case, a capacitor is connected from COMM1 to AC1 and from COMM2 to AC2. When the COMMx switches are closed there is effectively a 22 nF capacitor connected between AC1 and AC2. Connecting a capacitor in between AC1 and AC2 modulates the impedance seen by the coil, which will be reflected in the primary as a change in current.