JAJSEM8A June 2018 – April 2019 DRV5015
PRODUCTION DATA.
The DRV5015 samples the Hall element at a nominal sampling interval of every 16.67 µs to detect the presence of a magnetic north or south pole. At each sampling point, the device takes the average of the current sampled value and immediately preceding sampled value of the magnetic field. If this average value crosses the BOP or BRP threshold, the device output changes to the corresponding state as defined by the Overview section.
Figure 17 shows the DRV5015A1 propagation delay analysis in the proximity of a magnetic south pole. The Hall element of the DRV5015 experiences an increasing magnetic field as a magnetic south pole approaches near the device. At time t2, the average magnetic field is (B2 + B1) / 2, which is below the BOP threshold of the device. At time t3, the actual magnetic field has crossed the BOP threshold. However, the average (B3 + B2) / 2 is still less than the BOP threshold. As such, the device waits for next sample time, t4, to start the output transition through the analog signal chain. The propagation delay, td, is measured as the delay from the time the magnetic field crosses the BOP threshold to the time output transitions.
Figure 17. Propagation Delay