JAJSGR2 December 2018 INA240-SEP
PRODUCTION DATA.
By connecting one reference pin to VS and the other to the GND pin, the output is set at half of the supply when there is no differential input, as shown in Figure 26. This method creates a ratiometric offset to the supply voltage, where the output voltage remains at VS / 2 for 0 V applied to the inputs.