JAJSI39 October 2019 SN74HCS72-Q1
PRODUCTION DATA.
Phase relationships between waveforms were chosen arbitrarily. All input pulses are supplied by generators having the following characteristics: PRR ≤ 1 MHz, ZO = 50 Ω, tt < 2.5 ns.
For clock inputs, fmax is measured when the input duty cycle is 50%.
The outputs are measured one at a time with one input transition per measurement.
Figure 7. Voltage Waveforms, Setup and Hold Times
Figure 9. Voltage Waveforms, Input and Output Transition Times
Figure 6. Voltage Waveforms, Pulse Duration