JAJSEM1F March 2001 – August 2016 TLV2370 , TLV2371 , TLV2372 , TLV2373 , TLV2374 , TLV2375
PRODUCTION DATA.
A typical application for an operational amplifier is an inverting amplifier, as Figure 37 shows. An inverting amplifier takes a positive voltage on the input and outputs a signal inverted to the input, which results in a negative voltage of the same magnitude. In the same manner, the amplifier makes negative input voltages positive on the output. Select the input resistor (RI) and the feedback resistor (RF to add amplification.)
Figure 37. Application Schematic