JAJSFZ4E March 2009 – August 2018 TMS320C28341 , TMS320C28342 , TMS320C28343 , TMS320C28344 , TMS320C28345 , TMS320C28346
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
Figure 6-28 shows the OSC and PLL block.
Figure 6-28 OSC and PLL Block Diagram The on-chip oscillator circuit enables a crystal/resonator to be attached to the C2834x devices using the X1 and X2 pins. If the on-chip oscillator is not used, an external oscillator can be used in either one of the following configurations:
The three possible input-clock configurations are shown in Figure 6-29 to Figure 6-31.
Figure 6-29 Using a 3.3-V External Oscillator
Figure 6-30 Using a 1.8-V External Oscillator
Figure 6-31 Using the Internal Oscillator