JAJS280O October 2003 – March 2019 TMS320F2801 , TMS320F28015 , TMS320F28016 , TMS320F2802 , TMS320F2806 , TMS320F2808 , TMS320F2809
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
Figure 6-26 shows the OSC and PLL block on the 280x.
Figure 6-26 OSC and PLL Block Diagram The on-chip oscillator circuit enables a crystal/resonator to be attached to the 280x devices using the X1 and X2 pins. If the on-chip oscillator is not used, an external oscillator can be used in either one of the following configurations:
The three possible input-clock configurations are shown in Figure 6-27 through Figure 6-29.
Figure 6-27 Using a 3.3-V External Oscillator
Figure 6-28 Using a 1.8-V External Oscillator
Figure 6-29 Using the Internal Oscillator