JAJSPJ9 December 2022 TPS3435
PRODUCTION DATA
Make sure that the connection to the VDD pin is low impedance. Good analog design practice recommends placing a 0.1-µF ceramic capacitor as near as possible to the VDD pin. If a capacitor is not connected to the CRST pin, then minimize parasitic capacitance on this pin so the WDO delay time is not adversely affected.