JAJSFE6I July 2009 – May 2018 TPS65070 , TPS65072 , TPS65073 , TPS650731 , TPS650732
UNLESS OTHERWISE NOTED, this document contains PRODUCTION DATA.
The following events can reduce the charging current and increase the timer durations in the fast charge phase:
In each of these events, the internal timers are slowed down proportionately to the reduction in charging current. Note also that whenever any of these events occurs, termination detection is disabled.
A modified charge cycle with the thermal loop active is shown in Figure 29.
Figure 29. Thermal Loop