SLVSBR0C October 2014 – June 2015 TPS8268090 , TPS8268105 , TPS8268120 , TPS8268150 , TPS8268180
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS8268x device is a complete DC/DC step-down power supply optimized for small solution size. Included in the package are the switching regulator, inductor and input/output capacitors. Integration of passive components enables a tiny solution size of only 6.7mm2.
Figure 23. Typical Application Schematic
Figure 23 shows the schematic of the typical application. The following design guidelines provide all information to operate the device within the recommended operating conditions. An external input capacitor may be required depending on the source impedance of the battery or pre-regulator used to power TPS8268x. See also Power Supply Recommendations.
| Reference | Description | Manufacturer |
|---|---|---|
| IC1 | MicroSIP Module TPS8268xSIP | Texas Instruments |
| C1 | Tantalum Capacitor; T520B157M006ATE025; 150uF/6.3V | Kemet |
The TPS8268x allows the design of a complete power supply with no additional external components. The input capacitance can be increased in case the source impedance is large or if there are high load transients expected at the output. The dc bias effect of the input and output capacitors must be taken into account and the total capacitance on the output must not exceed the value given in the recommended operating conditions.
Because the nature of the buck converter has a pulsating input current, a low ESR input capacitor is required.
For most applications, the input capacitor that is integrated into the TPS8268x is sufficient. If the application exhibits a noisy or erratic switching frequency, experiment with additional input ceramic capacitance to find a remedy.
The TPS8268x uses a tiny ceramic input capacitor. When a ceramic capacitor is combined with trace or cable inductance, such as from a wall adapter, a load step at the output can induce ringing at the VIN pin. This ringing can couple to the output and be mistaken as loop instability or can even damage the part. In this circumstance, additional "bulk" capacitance, such as electrolytic or tantalum, should be placed between the input of the converter and the power source lead to reduce ringing that can occur between the inductance of the power source leads and CI.
The advanced fast-response voltage mode control scheme of the TPS8268x allows the use of tiny ceramic output capacitors. Ceramic capacitors with low ESR values have the lowest output voltage ripple and are recommended. For most applications, the output capacitor integrated in the TPS8268x is sufficient. An additional output capacitor may be used for the purpose of improving AC voltage accuracy during large load transients.
To further reduce the voltage drop during load transients, additional external output capacitance up to 30µF can be added. A low ESR multilayer ceramic capacitor (MLCC) is suitable for most applications. The total effective output capacitance must remain below 30µF.
As the device operates in PWM mode, the overall output voltage ripple is the sum of the voltage step that is caused by the output capacitor´s ESL and the ripple current that flows through the output capacitor´s impedance.
Because the damping factor in the output path is directly related to several resistive parameters (e.g. inductor DCR, power-stage rDS(on), PCB DC resistance, load switches rDS(on) …) that are temperature dependant, the converter´s small and large signal behavior should be checked over the input voltage range, load current range and temperature range.
The easiest test is to evaluate, directly at the converter’s output, the following items:
During the recovery time from a load transient, the output voltage can be monitored for settling time, overshoot or ringing that helps judge the converter’s stability. Without any ringing, the loop typically has more than 45° of phase margin.
Figure 24. Load Transient Response for TPS8268180
Figure 25. Line Transient Response for TPS8268180 
Figure 28. Load Transient Response for TPS8268150 
Figure 32. Load Transient Response for TPS8268120 
Figure 36. Load Transient Response for TPS8268105
Figure 38. Startup for TPS8268105
Figure 40. Load Transient Response for TPS8268090
Figure 42. Startup for TPS8268090
Figure 27. Output Voltage Ripple for TPS8268180
Figure 29. Line Transient Response for TPS8268150
Figure 31. Output Voltage Ripple for TPS8268150
Figure 33. Line Transient Response for TPS8268120
Figure 35. Output Voltage Ripple for TPS8268120
Figure 37. Line Transient Response for TPS8268105
Figure 39. Output Voltage Ripple for TPS8268105
Figure 41. Line Transient Response for TPS8268090
Figure 43. Output Voltage Ripple for TPS8268090