DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1 , DLPC231-Q1 , DLPC231S-Q1
The parameters for the available source configurations are stored in batch command sets in flash. To configure a source, the desired batch command set index should be executed. Once the batch command set is executed, the Prepare for Source Change command will disable illumination and the software will hold the configuration parameters until the Source Select command is sent. This two-command process provides time to prepare the external video source signals without displaying corrupted video data and causing the software to throw video source detection errors. During normal operation, an external video source should be adjusted between these two commands.
An image may only be displayed in Display Mode or Calibration mode.
The source change steps are summarized as follows:
If multiple external video inputs are used, the following steps must be used to switch between them. This assumes source 1 is being displayed: