DLPU077A March 2019 – June 2019 DLPC4422
Before programming the DLPLCRDC4422EVM, ensure the DLPC4422 GUI and DMD firmware are both downloaded on the PC. The DLPC4422 GUI will allow for operation of the EVM and the DMD firmware is required so the DLPLCRDC4422EVM knows which DMD is being controlled. If the DLPDLCR660TEVM is being used with the DLPLCRDC4422EVM, the DLP660TE firmware is needed. Else if the DLPDLCR470TEVM is used, the DLP470TE firmware is needed.
The DLP660TE firmware and DLPC4422 GUI can be found under the “Tools and Software” tab on the product pages on TI.com. These are the product pages for the DLP660TE, the DLP470TE, and the DLPC4422.