JAJSJT9A October 2020 – December 2020 LM7310
PRODUCTION DATA
The LM73100 implements undervoltage protection on IN in case the applied voltage becomes too low for the system or device to properly operate. The undervoltage protection has a default lockout threshold of VUVP which is fixed internally. Apart from that, the UVLO comparator on the EN/UVLO pin allows the undervoltage Protection threshold to be externally adjusted to a user defined value. The Figure 7-1 and Equation 1 below show how a resistor divider can be used to set the UVLO set point for a given voltage supply.
Figure 7-1 Adjustable Undervoltage
Protection