JAJSQM7C June 2023 – February 2025 BQ25628E
PRODUCTION DATA
The host may place the BQ25628E into ship mode by setting BATFET_CTRL = 10. In ship mode, the BATFET is turned off to prevent the battery from powering the system, and the I2C is disabled. Ship mode has slightly higher quiescent current than shutdown mode, but QON may be used to exit from ship mode. The BQ25628E is taken out of ship mode by either of these methods:
When the BQ25628E exits from ship mode, the registers are reset to their POR values.
Ship mode is only entered when the adapter is not present. Setting BATFET_CTRL = 10 while VVBUS > VVBUS_UVLOZ (adapter present) either disables the BATFET or has no immediate effect depending on the setting of BATFET_CTRL_WVBUS.